S32K118的pflash和dflash如何使用

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K118的pflash和dflash如何使用

跳至解决方案
698 次查看
Vapaus
Contributor III

S32K118的pflash和dflash如何配置并且使用

0 项奖励
回复
1 解答
671 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

在原帖中查看解决方案

0 项奖励
回复
4 回复数
250 次查看

thank u

0 项奖励
回复
672 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

0 项奖励
回复
350 次查看
Hello,which RTD version has the example?
0 项奖励
回复
326 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @重生之我在南京做牛码,

You can find the examples in RTD 2.0.0 for S32K1XX from the following page: Real-Time Drivers (RTD) | NXP Semiconductors.

Best regards,
Julián

0 项奖励
回复