CMU_FC destructive reset configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMU_FC destructive reset configuration

458 Views
FabioG
Contributor III

Hi There,

1) I looking for configuring CMU_FC peripheral (Chapter 54). Revision 8 of reference manual.

There no explicit reference (I don't find it ...) about setting destructive reset, but in logic network at Chapter 24, par 8 "Clock Monitoring, page 960 "Figure 115. Frequency checking (FC) instances"  seems that to enable destructive reset we have to enable asyncronous interrupts FHHAIE and FLLAIE as shown for FC4,5,3 is it true ?

2)And why for fc0 and Fc6, in order  to enable destructive reset is activated FHHIE (Syncronous Upper threshold!! ) on the LOWER threshold path , and  for the interrupt activation   is set FLLAIE (Lower Asyncronous)for the  UPPER threshold path  ? is it a mistake or a feature ? (see attached file)

2) in revision 5 of manual there was not present FC6 (CM7_CORE_CLK). what is the difference with FC3(CORE_CLK) ?

Best Regards

Fabio

0 Kudos
Reply
3 Replies

434 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FabioG,

1.

This is under an internal discussion at the moment.

2.

FC_6 is available on S32K388 only.

danielmartynek_0-1710242001591.png

 

Regards,

Daniel

0 Kudos
Reply

429 Views
FabioG
Contributor III

Regarding point 1: in order to checkCMU_FC  Distructive reset, what I need to configure in CMU_FC?

Best Regards,

Fabio

0 Kudos
Reply

414 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @FabioG,

Based on the latest update, the diagrams should be fixed in the next RM release.

Both FLL and FHH can generate either an interrupt or reset. The destructive reset is bond with the asynchronous mode, and the synchronous mode only generate the interrupt.

 

Regards,

Daniel

0 Kudos
Reply