S32DS CDT indexer get stucks when indexing and parsing a c file.
the debug log in the console is
Indexer: parsing \BCU_CODE\src\Cdd\CDD_Diag\CDD_Diag.c
Warning: NLS missing message: CdtProjectIndexerSettingsInitializer_set_description_to_project in: com.nxp.s32ds.ext.cdt.internal.validation.core.messages
Warning: NLS missing message: RefreshPolicyValidator_refresh_failed in: com.nxp.s32ds.ext.cdt.internal.validation.core.messages
then i adjust the vm size , and no waning output. but the indexer process still stucks, and the cpu load of s32ds is 20%+ (almost one cpu core)
any one can help?
已解决! 转到解答。
I am sorry that this is not the root cause. I changed the parameters before I post the issue.
further more, I have modified the VM arguments in s32ds.ini the increase the memory that coule be used.
but nothing works.