Hello, NXP support,
Now I am debugging CAN-FD&TJA1145FD using s32k144. The phenomenon is as follows.
S32K144 + CAN-FD + TJA1043
→CAN-FD communication(send/receive) is successful.
S32K144 + CAN + TJA1145FD
→CAN communication(send/receive) is successful.
S32K144 + CAN-FD + TJA1145FD
→CAN communication fails.
→PC CAN Box Tool displays “error frame" in output window.
→TJA1145FD 's TX pin has waveform, but it is different from the waveform of CAN-FD&TJA1043.
<Question>
Why does the communication fail when MCU uses CAN-FD&TJA1145FD ?
Is there any difference in the control method or configuration method of TJA1145FD when MCU uses CAN and CAN-FD?
With Best Regards,
已解决! 转到解答。
I have checked the CFDC of 20h.
CAN-FD comunication fails if CFDC = 0.
CAN-FD communcaiton also fails if CFDC = 1.
Hi chengsz,
Please check the CFDC of CAN control and Transceiver status registers. Here is the Data Sheet of TJA1145.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------