BUS OFF state can not be triggered

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BUS OFF state can not be triggered

Jump to solution
488 Views
witness
Contributor III

hi, experts

I am working on S32K324, and use below method test CAN bus off:

1) CANH connect to VCC

2) CANH connect to GND

3) CANL connect to VCC

4) CANL connect to GND

5) CANH connect to CANL

but the last case is failed, that means although CANH&CANL connected, the CAN bus off interrupt can not reached, can TXERRCNT does not increase, does anyone has encountered such issue?

0 Kudos
1 Solution
454 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@witness

First of all, if CAN-H and CAN-L are short-circuited during transmission, the node will definitely enter the bus-off state.

 

for one node:

there is only one transmission node on the bus, and it cannot get ACK from other nodes.

You can reproduce this situation,for example.

You can disconnect from the bus and then try to send a frame, then it will enter this state. At this time, if you connect CAN-L or CAN-H, it will not enter the bus-off state.

 

 

View solution in original post

0 Kudos
3 Replies
472 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@witness

please take a look at the S32K3XXRM_rev7->Chapter 74.6.2.8 Error Counter(ECR)

Senlent_0-1699943240089.png

You can try to test and short-circuit CAN-H and CAN-L during normal communication between the two nodes.

0 Kudos
461 Views
witness
Contributor III

hi, @Senlent 

Thanks for your reply. I am a little confused the concept for "two node", in fact, we are using Vector CANoe tool to do the test, and if we connect CANH to GND, the error frame will constantly occurs, so bus off state can be reached, but why CANH&CANL connect will not trigger bus off.

0 Kudos
455 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@witness

First of all, if CAN-H and CAN-L are short-circuited during transmission, the node will definitely enter the bus-off state.

 

for one node:

there is only one transmission node on the bus, and it cannot get ACK from other nodes.

You can reproduce this situation,for example.

You can disconnect from the bus and then try to send a frame, then it will enter this state. At this time, if you connect CAN-L or CAN-H, it will not enter the bus-off state.

 

 

0 Kudos