Dear Expert,
My purpose is to obtain a demo with FreeRTOS + LwIP, so I go to install TCPIP_STACK.
When I installed Package TCPIP_STACK _1_0_3, the following error occurred.
Before that, I had already installed several software packages on S32DS 3.5.
May I ask how to solve this problem?
Thanks.
suda
解決済! 解決策の投稿を見る。
Hi,
seems S32K396 development package is missing. Seems below thread is discussing this;
https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052
BR, Petr
Hi,
seems S32K396 development package is missing. Seems below thread is discussing this;
https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052
BR, Petr
hi
3q, this problem has been solved, I downloaded and installed the file SW32K39x_S32DS_3.5.6_D2309.zip.