An error occurred during the installation of the tcpip package TCPIP_STACK _1_0_3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

An error occurred during the installation of the tcpip package TCPIP_STACK _1_0_3

Jump to solution
451 Views
suda1684
Contributor I

Dear Expert,

  My purpose is to obtain a demo with FreeRTOS + LwIP, so I go to install TCPIP_STACK.  

  When I installed Package TCPIP_STACK _1_0_3, the following error occurred.

suda1684_0-1702003157855.png

 Before that, I had already installed several software packages  on S32DS 3.5.

  •   SW32K3_S32DS_3.5.8_D2311
  •   SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite
  •   SW32K3_FreeRTOS_10_5_1_UOS_3_1_0_DS_updatesite_D2304

May I ask how to solve this problem?

Thanks.
suda

0 Kudos
Reply
1 Solution
430 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

seems S32K396 development package is missing. Seems below thread is discussing this;
https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052

BR, Petr

View solution in original post

0 Kudos
Reply
2 Replies
431 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

seems S32K396 development package is missing. Seems below thread is discussing this;
https://community.nxp.com/t5/S32K/tcpip-1-0-3-can-t-be-installed/m-p/1686564#M25052

BR, Petr

0 Kudos
Reply
402 Views
suda1684
Contributor I

hi

  3q, this problem has been solved, I downloaded and installed the file SW32K39x_S32DS_3.5.6_D2309.zip.

0 Kudos
Reply