Recently, we confirmed that the linker file for S32K314 created with the newly created Application porect from S32DS was incorrect.
S32DS 3.4, NXP GCC 10.2 for Arm 32-bit Bare-Metal
RTD 2.0.0, Debugger Pemicro
The Length of ITCM and DTCM was incorrect, so I corrected it, but it seems that the Length of Flash is also incorrect.
The following is a comparison screen of the generated linker_flash_s32k314.ld file before (left) and after (right) modification.
The Length value of the flash area is also set to 0xD4000, but I think 0x3D4000 is correct.
please check this.
And, I will attach the linker file as an attachment. Please review to see if there are any other mistakes.
解決済! 解決策の投稿を見る。
Hi
Thank you for the report. Sorry for the inconvenience we bring you!
I checked linker_flash_s32k314.ld for S32K3 RTD 3.0.0 and this issue has been fixed.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
Thank you for the report. Sorry for the inconvenience we bring you!
I checked linker_flash_s32k314.ld for S32K3 RTD 3.0.0 and this issue has been fixed.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
能不能讲中文
Good. Thanks.