Hi,
CAN supports automatic retransmission function mentioned in CAN2.0 protocol,but I don't find it in FlexCAN User Guide document.Does FlexCAN support this function?
解決済! 解決策の投稿を見る。
Hi JihongZhang,
The FlexCAN module is a communication controller implementing the CAN protocol according to the ISO 11898-1 standard and CAN 2.0 B protocol specifications.
It supports automatic retransmission.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @Robin_Shen ,
Thank you for your answer.I want to know which register can enable this function?
There is no register to control this function.