About S32K144 FlexCAN automatic retransmission

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About S32K144 FlexCAN automatic retransmission

Jump to solution
1,065 Views
JihongZhang
Contributor II

Hi,

CAN supports automatic retransmission function mentioned in CAN2.0 protocol,but I don't find it in FlexCAN User Guide document.Does FlexCAN support this function?

 

0 Kudos
Reply
1 Solution
1,052 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

There is no register to control this function.

View solution in original post

0 Kudos
Reply
3 Replies
1,058 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JihongZhang,
The FlexCAN module is a communication controller implementing the CAN protocol according to the ISO 11898-1 standard and CAN 2.0 B protocol specifications.

It supports automatic retransmission.

55.2 Overview.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,055 Views
JihongZhang
Contributor II

Hi @Robin_Shen ,

Thank you for your answer.I want to know which register can enable this function?

0 Kudos
Reply
1,053 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

There is no register to control this function.

0 Kudos
Reply