AUTOSAR OS S32K1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

AUTOSAR OS S32K1

跳至解决方案
1,378 次查看
liuruowen
Contributor I

Hello:

I used S32K_AUTOSAR_OS_4_0_98_RTM_1_0_0 and got a problem, as shown below:

liuruowen_0-1600398059935.png

cannot generate the above files,what's the reason?

compiler:gccarm   Ver:4.9.3   Path:C:\NXP\S32DS_ARM_v2.2\S32DS\build_tools\gcc_v4.9\gcc-arm-none-eabi-4_9

GUN Make Ver:3.81

liuruowen_1-1600398339386.png

 

0 项奖励
回复
1 解答
1,364 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please make sure that you have installed Java 6.0 update 45 or higher, and the path to installed package are added into system environment:

Path_Java.JPG

Nam

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,365 次查看
namnguyenviet
NXP Employee
NXP Employee

Hello,

Please make sure that you have installed Java 6.0 update 45 or higher, and the path to installed package are added into system environment:

Path_Java.JPG

Nam

0 项奖励
回复