ADC project using MCAL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC project using MCAL

1,301 次查看
laofu
Contributor II

HI,@NXP

I try to build a ADC project triggered by pdb using s32ds with autosar mcal,whether just the mcal module ADC is needed,should the drivers module Adc_Ip and pdb_Adc_Ip is needed? thanks

laofu_0-1678906669186.png

 

0 项奖励
7 回复数

1,266 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Hi,
If you added Adc in MCAL module, don't need to add PDB_Adc_Ip under Driver layer

0 项奖励

1,251 次查看
laofu
Contributor II

thinks for your replying,I want the pdb trigger by Lpit ,but in mcal ADC module,i can not configure the pdb to trigger by hardware,it seems that pdb  can only triggered by software.My ultimate aim is just using mcal to configure a project that adc is triggered by pdb ,and pdb is triggered by Lpit.

 

0 项奖励

1,134 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Sorry for late response,
I created the example ADC trigger by LPIT in the attached file and the guidance to configure and implement for example. please look at these attachments

0 项奖励

1,117 次查看
laofu
Contributor II

HI,thanks.does the example project you provided is mistake? it seems about i2c.  in addition,my RTD is 1.01and this example use RTD1.0.0, so i can not open it

0 项奖励

1,106 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Sorry, I make mistake when upload the example
I re-attached the ADC project for K1 RTD 1.0.1

0 项奖励

1,237 次查看
cuongnguyenphu
NXP Employee
NXP Employee

Can you give me the information of hardware target and RTD version you're using?

0 项奖励

1,229 次查看
laofu
Contributor II

Hi,

i use the s32k144,and RDT version is 1.0.1.

0 项奖励