AD detection is not allowed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AD detection is not allowed

1,192 次查看
ywjack
Contributor III

The accuracy of the ADC is not accurate. I used the ADC0 channel 13 (PTC15) to detect the voltage. But I found that the 3.3V is the ADC value is 1023, (ten-bit resolution), but I detected 2.5V is the ADC value of 808, already The 0.1V is worse. What's even more strange is that the ADC value I detected for 0.5V is 78. This variation is already very large. Can help me check if my location problem or other problem, I will attach my code configuration

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,118 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello ywjack@126.com,

Is the ADC module calibrated?

Do you use an EVB or your custom board?

Please measure VREFH, VREFL voltage.

Thank you,

BR, Daniel

0 项奖励
回复