Example of usage of AIPS-lite, Protects the access to GPIO port. This example can be used with UART terminal, 115200 bps. The interface menu shows like this:
AIPS example has started
Please press 0 + enter to set red LED in GPIO port
Please press 1 + enter to set red LED in GPIO port
Please press 2: GPIO peripheral will only accept accesses from trusted master, M0 (Core) is set as untrusted when a write access, AIPS cannot longer be modified from core and a reset will occur in the next GPIO access
Please press 3: GPIO access is write protected, any write access to GPIO will produce a hard fault