Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300

Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of the
 UART IP Driver for the S32K3xx MCU.

 The example uses LPUART6 for transmit & receive five bytes using the DMA.


 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-T172
* MCU: S32K344
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE micro
* Target: internal_FLASH
********************************************************************************

Dinesh_Guleria_0-1718197381145.png

 



Dinesh_Guleria_1-1718197381161.png

 

Putty output :--

Dinesh_Guleria_2-1718197434242.png

 

添付
コメント

@Dinesh_Guleria  do you have an example of DMA UART in RTD 4.0.0?

Hi @Dinesh_Guleria ,

 

Can we use DMA without Autosar (RM CDD)? 

評価なし
バージョン履歴
最終更新日:
‎06-12-2024 06:04 AM
更新者: