********************************************************************************
* Detailed Description:
*
* This example shows how to use the back-to-back mode of the PDB to trigger
* sequence of ADC channels conversion. 4 PDB channel 0 pre-triggers/triggers are
* generated upon single PDB SW trigger. The first trigger is started by the PDB,
* no delay is used. Next 3 triggers start after corresponding acknowledgment is
* received from ADC0.
*
* Converted data is used to change color of the EVB led based on Trimmer position.
*
* ------------------------------------------------------------------------------
* Test HW: FRDM-S32K144
* MCU: PS32K144HFVLL 0N77P
* Fsys: default
* Debugger: S32DS
* Target: internal_FLASH
*
********************************************************************************