What is the compatible pfe firmware version of bsp35?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the compatible pfe firmware version of bsp35?

996件の閲覧回数
irfank
Contributor III

We are using bsp35 and pfe1.5. It depends on release note:

irfankarazor_1-1691074481316.png

 

 

 

There is a error as seen below?

irfankarazor_0-1691074650104.png

 

 

0 件の賞賛
返信
4 返答(返信)

839件の閲覧回数
irfank
Contributor III

Thanks you for your support, It was my fault.

972件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

For BSP35.0, PFE-FW v1.5.0 is the one compatible with. For the log that you are showing, we see that the u-boot version is a newer one than the one we have under our BSP35.0 image:

DanielAguirre_0-1691089343184.png

For which we assume you are building your own image. How are you building your image? Can you confirm which version you are building?

Please, let us know.

0 件の賞賛
返信

930件の閲覧回数
irfank
Contributor III

Hello,

We compile our image by yocto. 

Start commit of our  Uboot code  is https://github.com/nxp-auto-linux/u-boot/commit/f30287c440b5371df683aac37b7521048d164d05.  then we update it depends on our board. 

If we use same uboot code under bsp33 with pfe1.3. It is ok.

But If we use this uboot code with bsp35 with pfe1.5. We have the above error.

If we use this uboot with bsp35 with pfe1.3 . uboot is bring up, but pfe is not connect network.

 

irfankarazor_0-1691131989778.png

 

0 件の賞賛
返信

898件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We might not be understanding. You use the BSP33.0 u-boot branch and PFE-FW 1.3 and it works, but you use your same image and BSP35.0 u-boot branch and PFE-FW 1.5 and it does not work, is this correct?

Which BSP base is your image? We understand that you are only changing the u-boot but your base image is the same, which we assume is BSP33.0, is this correct?

Please, let us know.

0 件の賞賛
返信