Hi experts,
I noticed that the BSP35 rc7 has been released for S32G, but when I tested it,
I found that the boards(EVB/RBD2/RDB3) can not boot with the HSE enabled, the logs as below:
NOTICE: Reset status: Destructive Reset (RUN)
NOTICE: BL2: v2.5(release):bsp34.0-2.5-84-g87dcc306a
NOTICE: BL2: Built : 07:11:12, Sep 6 2022
For clear, the "NOTICE: BL2: v2.5(release):bsp34.0-2.5-84-g87dcc306a" is still bsp34 tag, because the bsp35 is not officially released now, but the patches of BSP35 rc7 have all been applied.
Would you please help to check and confirm the issue?
Thanks,
Zhantao
Solved! Go to Solution.
Hi Daniel,
This issue is caused by the following patch in atf repo:
commit 4f6132d25c986c437dc9eb89fa8489ea5b97a05b
Author: Vlad Pelin <vlad.pelin@nxp.com>
Date: Tue Nov 8 17:58:30 2022 +0200
secboot: add support for userspace secboot
handling secure boot in userspace means that some
changes made to atf are no longer needed
Issue: ALB-9004
Signed-off-by: Vlad Pelin <vlad.pelin@nxp.com>
Please talk to the development team, they will know what happened with the commit.
Thanks,
Zhantao
Hi,
As you are saying, BSP35 is not released at this moment (BSP34 is not officially available for download also, at this moment).
We cannot find any notice about problems with HSE at this point in time, we will send this notice to the development team. Due to BSP35 being in early release, could be that not all changes are implemented at this moment.
Please, let us know if this information was helpful or not.
Hi Daniel,
This issue is caused by the following patch in atf repo:
commit 4f6132d25c986c437dc9eb89fa8489ea5b97a05b
Author: Vlad Pelin <vlad.pelin@nxp.com>
Date: Tue Nov 8 17:58:30 2022 +0200
secboot: add support for userspace secboot
handling secure boot in userspace means that some
changes made to atf are no longer needed
Issue: ALB-9004
Signed-off-by: Vlad Pelin <vlad.pelin@nxp.com>
Please talk to the development team, they will know what happened with the commit.
Thanks,
Zhantao
Hi,
Thanks for the notice, will provide the feedback to the development team.
Have a great day.