Running freertos multicore M7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Running freertos multicore M7

133 次查看
Aswin_Devaraj
Contributor I

Hi, 

I am using the S32G VNP RDB3 board.

Have installed the latest packages from NXP package manager for S32g.

I was able to run freertos on M7_0 core....

Now I want to run freertos on M7_0 and M7_1 core and want to split the peripherals among these cores...

like ADC for core0, PWM for core1 and

LLCE can0 and can1 for core0, LLCE can14 and LLCE can15 for core 1.

So.. I want to know how to handle freertos in multicore... Is there any demos or documents that I can refer....

If not please suggest some ideas on how to handle M7 multicore SW using Design Studio.

S32G3 

0 项奖励
1 回复

111 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

On regards of documentation/examples on how to handle sharing resources under a multicore application, we understand that there are no official public documents/examples. We see though the following community knowledge base:

S32G Bootloader Customzition - NXP Community

Which provides a general idea of resource sharing and conflicts.

If more information is required, we can recommend contacting your local NXP FAE/DFAE/representative, or opening a ticket under the NXP online services, for them to verify if there is any more information available to this topic.

Please, let us know.

0 项奖励