Not able to edit a ETH_43_PFE Parameter in EB Tresos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Not able to edit a ETH_43_PFE Parameter in EB Tresos

1,203件の閲覧回数
Kanika
Contributor II

Hi,

I am trying configure CAN2ETH routing in EB Tresos and while trying to verify the Eth Module I am getting the attached errors.

Moreover, when I tried to fix the error the parameter EthCtrlConfigIngressFifoBufLenByte in Eth_43_PFE is disabled for edit(screenshot attached).

Please let me know how can I enable this parameter to set the correct range as the error is for out of the range value or is there any depending parameter which I need to change to set this value or make it enable.

 

0 件の賞賛
返信
3 返答(返信)

1,174件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are not seeing this behavior on our setup. Image below:

DanielAguirre_0-1682706652304.png

 

Our current setup is the following:

  • Tresos 28.2
  • LLCE v1.0.4
  • RTD 3.0.2 HF01
  • PFE v0.9.7

Which versions are you using currently?

Please, let us know.

0 件の賞賛
返信

1,168件の閲覧回数
Kanika
Contributor II

Tresos:28.2

LLCE :1.0.5

PFE : 1.0.0

RTD :4.0.0

0 件の賞賛
返信

1,121件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

This seems to be a known issue under the versions that you are using. The following modifications need to be made:

DanielAguirre_0-1682964352672.png

There is a typo on the presentation (it mentions 2049 instead of 2048), but the modification is valid. With that, you obtain the following result:

DanielAguirre_1-1682964409346.png

Please, let us know.

0 件の賞賛
返信