Hi,
We understand that you are trying to implement a multicore application under the S32G2 platform. If so, we recommend reading AN13750 since this is the only multicore demo available under S32G2. The files needed are available under the S32G2 product page (link: S32G2 Safe and Secure Vehicle Network Processor | NXP Semiconductors) in the "Documentation" section, both the AN13750 and the AN13750SW.
Inside the AN13750, all steps needed to implement a multicore application are provided. The patches and projects (not including the bootloader, which AN13750 tells where to find it) required are provided in the AN13750SW.
S32G2 has a kind of unique boot process, in which the integrated BootROM only starts 1 core, all the other cores have to be configured and started from this single online core, which has to be done by the developer. We can recommend looking into the AN12422 available under the S32G2 product page (link above) for an overview on the S32G2 boot process.
Also, Figure 152 [Page 1083, S32G2 Reference Manual, Rev. 6, 11/2022] inside the Reference Manual provides a sequence on how to start additional cores.
We can also recommend reading "Chapter 32 Mode Entry Module (MC_ME)" [Page 1219, S32G2 Reference Manual, Rev. 6, 11/2022] which provides a little more detail on the required registers for a multicore boot (on regards of clock enable, start address, etc...).
Please, let us know if there is anything else we can help you with.