GoldBox-3 physicals and electrical information

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GoldBox-3 physicals and electrical information

ソリューションへジャンプ
311件の閲覧回数
Shrek78
Contributor I

Hello,

Is there any information on physicals and electrical interfaces for the GoldBox-3?

  • Acceleration / Vibrations / Stiffness resistance based on specific standart
  • Min Max for temperature and humidity
  • Power consumption
  • electromagnetic compatibility (EMC)
  • is it rugged
0 件の賞賛
返信
1 解決策
292件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that this information is not provided. We do apologize.

The information that may be available is on regards of temperature, which is the following (only for RDB2):

"RDB2 is designed for room temperature environment.

The board may work abnormally or be damaged in the high/low temperature test."

And about rugged (we think so?):

DanielAguirre_0-1707922050902.png

Still, help us contacting your local NXP representative/FAE/DFAE, since they may more information available than the one we have through this channel. We do apologize.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
293件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We understand that this information is not provided. We do apologize.

The information that may be available is on regards of temperature, which is the following (only for RDB2):

"RDB2 is designed for room temperature environment.

The board may work abnormally or be damaged in the high/low temperature test."

And about rugged (we think so?):

DanielAguirre_0-1707922050902.png

Still, help us contacting your local NXP representative/FAE/DFAE, since they may more information available than the one we have through this channel. We do apologize.

Please, let us know.

0 件の賞賛
返信