Creating M7 firmware image with IVT for S32G2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating M7 firmware image with IVT for S32G2

1,662件の閲覧回数
yellapu_anishkh
Contributor IV

I am using BSP28, which compiles linux and u-boot.

u-boot with IVT is created, similarly M7 binary with IVT has to be created.

Please point me with the process to compile M7 binary and create IVT for M7 binary

0 件の賞賛
返信
1 返信

1,639件の閲覧回数
bpe
NXP Employee
NXP Employee

You need S32 Development Studio with support to S32G2 processors installed to
generate IVT for M7 cores. Automotive BSP cannot do it, it has no support to M7 cores.
Familiarize yourself with the document at this link, slides 3 through 24 to see how to
create a bootable image for M7 core. That includes IVT generation.

Hope this helps,
Platon

 

 

0 件の賞賛
返信