Hi, I use lin slave sdk example in S32 Design Studio for ARM v1.3
I was having trouble reading the Lin_slave.dox document in the Doxtgen folder.
I use S32K144EVB-Q100. But, What does S32K144-MB mean?
And
PIN FUNCTION | S32K144EVB-Q100 | S32K144-MB
----------------|---------------|--------------
BUTTON 2 (\b PTC13) |BTN1 - wired on the board | BTN3 - wired on the board
BUTTON 1 (\b PTC12) |BTN0 - wired on the board | BTN2 - wired on the board
RED_LED (\b PTD15) |RGB_RED - wired on the board | J12.17 - J11.31
GREEN_LED (\b PTD16) |RGB_GREEN - wired on the board | J12.16 - J11.30
BLUE_LED (\b PTD16) |RGB_GREEN - wired on the board | J12.31 - J11.29
GND (\b GND) |J3-11 - Master GND |J6 - Master GND
LPUART2_RX (\b PTD6) |J5-18 - J4-6 | J12.25 - J10.17
FTM0_CH5 (\b PTB17) |J4.6 - J5.18 | J10.17 - J12.25
LIN (\b *) |J11-1 - Master LIN | J48.4 - Master LIN
<b>(*) Those lines must be modulated using a transceiver, if it is not specified the boards already include the LIN transceiver</b>
GND (\b GND) |J3-11 - Master GND |J6 - Master GND
LPUART2_RX (\b PTD6) |J5-18 - J4-6 | J12.25 - J10.17
FTM0_CH5 (\b PTB17) |J4.6 - J5.18 | J10.17 - J12.25
LIN (\b *) |J11-1 - Master LIN | J48.4 - Master LIN
What does it mean?
解決済! 解決策の投稿を見る。
Hi,
Yes, you have to connect them using a cable from J5-18 - J4-6(on the board headers).
Best regards,
Rares
Hi,
The S32K144-MB is an internal board, used for validation.
Best regards,
Rares
Hi,
Do I need to connect the two wires?
LPUART2_RX (\b PTD6) |J5-18 - J4-6 | J12.25 - J10.17
FTM0_CH5 (\b PTB17) |J4.6 - J5.18 | J10.17 - J12.25
Thank you.
Hi,
Yes, you have to connect them using a cable from J5-18 - J4-6(on the board headers).
Best regards,
Rares