SPI ( FLEXIO SPI, LPSPI)COM between two S32K MICROCONTROLLERS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI ( FLEXIO SPI, LPSPI)COM between two S32K MICROCONTROLLERS

Jump to solution
1,853 Views
saidbenlahmadi
Contributor I

Hello everybody, 

I want to communicate between two MCUs(S32K) via SPI: 

Master use LPSPI and the slave use FLEXIO SPI. 

Is there any way to configure the FLEXIO SPI driver to trigger an interrupt once the master finish the communication to read data by slave? 

Do you have any other idea to exchange the data between the two MCUs other then interrupts ?  

Labels (2)
0 Kudos
Reply
1 Solution
1,847 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, FlexIO SPI driver support DMA, so you can configure DMA to generate interrupt at the end of the major loop. This would assume messages with constant length.

 

View solution in original post

0 Kudos
Reply
1 Reply
1,848 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, FlexIO SPI driver support DMA, so you can configure DMA to generate interrupt at the end of the major loop. This would assume messages with constant length.

 

0 Kudos
Reply