S32R294_RSDK_1_3_0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R294_RSDK_1_3_0

2,317件の閲覧回数
tyson1
Contributor I

Hi ,

    I installed the software for SWS32R294_Radar_SDK_1.3.0_D2105.exe in path C:\NXP

  But when I open the example in the S32 Design Studio for Power Architecture Version 2.1,create S32DS PROJECT FROM EXAMPLE ,import RSDK_Multi_RFE_example_S32R294,show File not found: /RSDK_Multi_RFE_example_S32R294/src/core0/main_c0.c.

The problem is that there are files in the RSDK path, but not in the workspace after import, so which step is wrong

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,136件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Latest info is that next release is in mid August and they will take care of the issue there.

Best regards,
Peter

0 件の賞賛
返信

2,309件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

From your description it looks like all you need to do is to set correctly path to the source files in your project.

Could you post some screenshots of the errors?

Best regards,

Peter

0 件の賞賛
返信

2,307件の閲覧回数
tyson1
Contributor I

S32R294_RSDK__1_3_0   path in C:\NXP

 

0 件の賞賛
返信

2,302件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I was talking with RSDK team, they will debug the issue in following days.

I will update you ASAP.

best regards,

Peter

0 件の賞賛
返信