S32K148 PDB ADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
932件の閲覧回数
QJ_HAPPY
Contributor I

HI:

When I configure the BACK-TO-BACK mode of PDB, can I only configure channels 0-7 in sequence, but not remove channels from the middle ?

Thanks

 

ラベル(1)
0 件の賞賛
返信
1 解決策
927件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please read the "46.1.3 Back-to-back acknowledgement connections" and "Figure 46-5. PDB-ADC back to back con": Back-to-back operation enables the ADC conversions complete to trigger the next PDB channel pre-trigger and trigger output.

Back-to-back acknowledgement connections.png

There is no such possibility that Pre-trigger 0 COCO is directly connected to Pre-trigger 2.

Figure 46-5. PDB-ADC back to back connection.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
928件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please read the "46.1.3 Back-to-back acknowledgement connections" and "Figure 46-5. PDB-ADC back to back con": Back-to-back operation enables the ADC conversions complete to trigger the next PDB channel pre-trigger and trigger output.

Back-to-back acknowledgement connections.png

There is no such possibility that Pre-trigger 0 COCO is directly connected to Pre-trigger 2.

Figure 46-5. PDB-ADC back to back connection.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

919件の閲覧回数
QJ_HAPPY
Contributor I
I understand now. Thank you for your reply
0 件の賞賛
返信