Hi,
So recently I´ve been having a strange problem with the Buffer Descriptor array, so basically when the MAC gets to the last position of the BD array I stop receiving new data (no more interrupt is generated) and I have no idea why as I´m using the UDP example that comes with the IDE, I also have checked the PING example where it works fine and I have the same configurations, when I process the new data I´m writing the E bit back to 1 to mark the BD as free but the mac stops at the last position of the ring and never gets back to the first position.
The number of messages I´m able to get its equal to the size of my buffer descriptor array´s size.
I attached the code to this question and I´d appreciate any help as I´m running out of ideas on what might be the problem.
Kind regards,
Lopes
已解决! 转到解答。
this will be caused by enabled data cache. Buffer descriptors should be placed in non-cachable region.
So either disable cache in startup or configure ceitain memory as cache inhibited using SMPU as mentioned here:
https://community.nxp.com/message/818983?commentID=818983#comment-804432
BR, Petr
Hi,
seems you set start address of descriptiors in ENET_RDSR to the non used one. You have defined rxdb and rx2bd descriptor rings but work with rxdb. Also the only rxdb last descriptor has Wrap bit set.
But ENET_RDSR points to rx2db[0].
BR, Petr
this will be caused by enabled data cache. Buffer descriptors should be placed in non-cachable region.
So either disable cache in startup or configure ceitain memory as cache inhibited using SMPU as mentioned here:
https://community.nxp.com/message/818983?commentID=818983#comment-804432
BR, Petr
Hi PetrS thank for the reply,
Actually I made a mistake there and forgot to change back to the rxdb instead of the rx2db as I was trying to see if setting it to an other buffer would work, but even with the ENET_RDSR pointer set to rxdb its not working.
Here´s the old version of the code, where I'm doing everything the same as in the original example but when i get x messages and x= size of my bd array the driver never gets an other message. In this one by bd size is set to 20 ( NUM_RXBDS 20 in eth_conf.h)
so I'm only getting 20 frames.
Again thanks for the reply and sorry for the mistake with the code.