Hi,
How to enable the driver for the FS4500 SBC with the S32 SDK RTM 3.0.2 ? I don't see the item in the Processor Expert component library window.
Regards,
Snaku
解決済! 解決策の投稿を見る。
Thanks for this picture.
The problem is that you still don't have the right Processor Expert repository because probably CPU component version is 09, not 15.
You can fix this in 2 ways.
Please start a new project from our example code from RTM 3.0.0 (File-> start new project from examples).
Go in Components view-> right click on each component -> Change repository and select the right version.
Best regards,
Razvan
Hi,
Which CPU are you using in your project?
FS45 was tested just in context of S32K148.
Best regards,
Razvan
Hi Razvan,
I am using S32K144.
I tried to create a new project with S32K148, but the FS4500 doesn't in the component list.
Does the FS4500 need any special feature from S32K148? the driver should be compatible with S32K144, right?
Regards,
Snaku
Hi,
I can't reproduce this issue. Are you sure that you are using the RTM 3.0.2?
How did you installed it?
Best regards,
Razvan
Hi Razvan,
I install the RTM 3.0.2 via 'install New Software...' of the 'help' menu, I install the RTM SDK 3.0.0 and RTM 3.0.2 patch.
[ my installed software ]
It could be my installation issue, because after I install the RTM 3.0.2, I find the Repositories path of the Process Expert still use SDK_S32K14x_09 only, I have to add the path for SDK_S32K14x_15 manually, and deselect the SDK_S32K14x_09 checkbox.
[ Processor SDK ]
Is there any way can check my SDK installed is correctly or not?
Regards,
Snaku
Hi,
Did you tried to create a new work space after the update was installed?
Razvan
Hi Razvan,
I change my worksapce to a new folder, and create a new project with S32K148, but there still has no FS4500 component.
I check the RTM 3.0.2 release note again, it states "BC_FS45: FS45_LIN_SetMode function is not supported for this release. In code this function is available, but it is up to the user to enable it by defining FS45_FEATURE_LIN macro in the driver.", Does it mean that FS45 driver will not show on the component inspector?
By the way, I can find the source code folder, sbc_fs45, on my computer. The path is C:\NXP\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_RTM_3.0.0\middleware\sbc\sbc_fs45.
Regards,
Snaku
Thanks for this picture.
The problem is that you still don't have the right Processor Expert repository because probably CPU component version is 09, not 15.
You can fix this in 2 ways.
Please start a new project from our example code from RTM 3.0.0 (File-> start new project from examples).
Go in Components view-> right click on each component -> Change repository and select the right version.
Best regards,
Razvan
Hi Razvan,
Yes, you are right, I can see the sbc_fs45 component now, and like you said, it only appear when the MCU is S32K148 with SDK_S32K1xx_15 repository, not support with S32K144.
Thank you,
Snaku