About the installation folder of S32K1_ISELED_BETA_2.9.2.exe

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About the installation folder of S32K1_ISELED_BETA_2.9.2.exe

跳至解决方案
1,770 次查看
r_kikuchi
Contributor I
This page (https://iseled.com/products.html)
Refer to the NXP Installation Guide (S32K SDK ISELED Driver installation guide BETA 2.9.2.pdf)
ISELED Software (S32K1_ISELED_BETA_2.9.2.exe) was obtained from NXP.
1. Please tell me where to specify the folder after executing S32K1_ISELED_BETA_2.9.2.exe.
2. Please tell me the work content of "Note: Please make sure you uninstall previous SDK so that this variable will be empty."
标记 (4)
0 项奖励
回复
1 解答
1,587 次查看
dragosrachitan
NXP Employee
NXP Employee

Hello,

The ISELED driver should be installed over the S32K1xx_SDK_BETA_2.9.2 release that you previously installed. As I can see from your folder tree, you should select the folder from S32DS\S32SDK_S32K1xx_BETA_2.9.2

Best regards,

Dragos

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,588 次查看
dragosrachitan
NXP Employee
NXP Employee

Hello,

The ISELED driver should be installed over the S32K1xx_SDK_BETA_2.9.2 release that you previously installed. As I can see from your folder tree, you should select the folder from S32DS\S32SDK_S32K1xx_BETA_2.9.2

Best regards,

Dragos

0 项奖励
回复
1,587 次查看
r_kikuchi
Contributor I
Thank you.

A1. I was able to install safely.
A2. After installation, "S32DK_PATH -> C:\NXP\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_BETA_2.9.2" is added to the system environment variable.
0 项奖励
回复