Hello,
If I configure a pin as EIRQ (not GPIO), can I still use API Siul2_Dio_Ip_ReadPin to read it?
Thanks.
解決済! 解決策の投稿を見る。
Hi
When a pad is configured to use one of its alternate functions, the data input values reflect the respective value of the pad.
So I think you can still use API Siul2_Dio_Ip_ReadPin to read it.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
When a pad is configured to use one of its alternate functions, the data input values reflect the respective value of the pad.
So I think you can still use API Siul2_Dio_Ip_ReadPin to read it.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------