Siul2_Dio_Ip_ReadPin & EIRQ

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Siul2_Dio_Ip_ReadPin & EIRQ

Jump to solution
2,396 Views
jetty_1012
Contributor II

Hello,

 

If I configure a pin as EIRQ (not GPIO), can I still use API Siul2_Dio_Ip_ReadPin to read it?

 

jetty_1012_0-1697187782378.jpegjetty_1012_1-1697187828887.jpeg

 

Thanks.

0 Kudos
Reply
1 Solution
2,384 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

When a pad is configured to use one of its alternate functions, the data input values reflect the respective value of the pad.

So I think you can still use API Siul2_Dio_Ip_ReadPin to read it.

When a pad is configured to use one of its alternate functions, the data input values reflect the respective value of the pad..png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,385 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

When a pad is configured to use one of its alternate functions, the data input values reflect the respective value of the pad.

So I think you can still use API Siul2_Dio_Ip_ReadPin to read it.

When a pad is configured to use one of its alternate functions, the data input values reflect the respective value of the pad..png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply