S32K3 Sample Projekts (S32Kx4EVB-Q257)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K3 Sample Projekts (S32Kx4EVB-Q257)

ソリューションへジャンプ
2,134件の閲覧回数
JoDo
Contributor III

Hello, I have a S32Kx4EVB-Q257 Evalboard and I am trying to get the board working. I have installed the S32K3xx development package (SW32K3_S32DS_3.4.1_D2108.zip). However, I can't find any sample projects or use the configuration tool. Is there any additional software or packages that need to be installed?

I have installed:

S32 Design Studio 3.4
GDB Client for ARM Embedded Processors 9.2 Build 1701
NXP GCC for ARM Embedded Processors Build 1620
NXP GCC for ARM Embedded Processors Build 1649
S32 Design Studio Platform Package v 3.4.1
S32 Design Studio Platform Tools Package v 3.4.1
S32K3xx development package v3.4.1 EAR1
S32K3 FreeMaster Serial Communication driver v3.0

0 件の賞賛
返信
1 解決策
2,117件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JoDo,

You need to download and offline install S32K3 Real Time Drivers
DFAE should give you a link to download RTD and S32DS.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,118件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JoDo,

You need to download and offline install S32K3 Real Time Drivers
DFAE should give you a link to download RTD and S32DS.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信