S32K3 Sample Projekts (S32Kx4EVB-Q257)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Sample Projekts (S32Kx4EVB-Q257)

Jump to solution
1,939 Views
JoDo
Contributor III

Hello, I have a S32Kx4EVB-Q257 Evalboard and I am trying to get the board working. I have installed the S32K3xx development package (SW32K3_S32DS_3.4.1_D2108.zip). However, I can't find any sample projects or use the configuration tool. Is there any additional software or packages that need to be installed?

I have installed:

S32 Design Studio 3.4
GDB Client for ARM Embedded Processors 9.2 Build 1701
NXP GCC for ARM Embedded Processors Build 1620
NXP GCC for ARM Embedded Processors Build 1649
S32 Design Studio Platform Package v 3.4.1
S32 Design Studio Platform Tools Package v 3.4.1
S32K3xx development package v3.4.1 EAR1
S32K3 FreeMaster Serial Communication driver v3.0

0 Kudos
Reply
1 Solution
1,922 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JoDo,

You need to download and offline install S32K3 Real Time Drivers
DFAE should give you a link to download RTD and S32DS.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,923 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JoDo,

You need to download and offline install S32K3 Real Time Drivers
DFAE should give you a link to download RTD and S32DS.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply