Hi all.
I'm working with S32K116 device and RTD from NXP.
i'm shocked regarding size of generated drivers...
Adding 3/4 RTD drivers [adc; i2c; pwm; can; timer...], not MCAL, lead to have more than 60% of RAM and Flash occupied
Maybe I have miss configure something. Please don't hesitate if you have some tips
I have another question, FlexRam usage.
I understood risk as there is no ECC.
I'm able to create memory region in the linker file and perform basic usage of it.
int_flexRam : ORIGIN = 0x14000000, LENGTH = 0x000007FF /* FlexRam Space */
volatile uint32_t __attribute__((section(".flexram"))) u32MyVar[10] ;
I would like to tel the linker to use the FlexRam in addition to the sram.
Is there a way to do something like bellow?
{
/* data, bss,... sections*/
} > int_sram, int_flexram
Thanks in advance for your answers.
Regards.