S32DS3.4 debug configuration Ram Application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS3.4 debug configuration Ram Application

ソリューションへジャンプ
1,346件の閲覧回数
tianxing
Contributor III

tianxing_0-1639466875113.png

What does the Ram application mean?

If not select Ram application S32DS cannot debug and always has the warrning that Failed to read memory @ address 0x20020000

 

 

0 件の賞賛
返信
1 解決策
1,325件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

if you are using RAM target application - (instead of FLASH target) after reset your binary disappears from RAM. With this option enabled - after reset is your binary again upload into RAM. 

 

Jiri 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,326件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

if you are using RAM target application - (instead of FLASH target) after reset your binary disappears from RAM. With this option enabled - after reset is your binary again upload into RAM. 

 

Jiri 

0 件の賞賛
返信
1,313件の閲覧回数
tianxing
Contributor III

Hi

I am using Flash target application. What's the difference between with Ram Application and without Ram Application?

0 件の賞賛
返信
1,300件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

This option is ignored for Flash target application. 

 

Jiri

0 件の賞賛
返信