S32DS for S32 platform installer stuck forever after entering activation code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS for S32 platform installer stuck forever after entering activation code

1,157 次查看
Joao_Roscoe
Contributor III

I'm trying to install S32DS for S32 platform (S32DS.3.5_b220726_linux.x86_64.bin) onto a Ubuntu 22.04.3 LTS box. I launched the installer as a regular user, and got a sudo passwd prompt (console) and a activation code prompt (java popup window), and answered both of them. All I got was a stuck installer - see attached snapshot. Could not find any other popup window.

Any hints?

Best regards, 

João

 

 

0 项奖励
回复
5 回复数

729 次查看
amitwarbhe
Contributor I

Even with admin privileges I am facing the same issue.

Activation Code:1992-D57A-4A33-66CA

0 项奖励
回复

964 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Joao_Roscoe , 

Please let us know if you were able to further with the S32DS installation. 

Thank you, Best regards, 

- Mehul Patel

0 项奖励
回复

1,098 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Joao_Roscoe , 

 

Please make sure that you have administrator right privileges while installing the S32DS. 

If you having problem with admin rights, please can you check with your company's It team. 

1. And once again try to steps as mentioned in the guide : https://www.nxp.com/webapp/Download?colCode=S32DSIG

 

2. Or you may you try offline activation method as per this page

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Activate-S32-Design-Studio/ta-p/...

 

If both, doesn't work: 

Please can you share your activation code so I can check if activation request reached to server or not. 

 

And, please can you share workspace details and installation log:

S32DS installation log: C:\NXP\S32DS.3.5\_S32 Design Studio for S32 Platform 3.5_installation\Logs

(or wherever the installation directory located) 

 

Also, Please check this post: 

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Troubleshooting-Activation-fails-with-...

 

 

Thank you. Best regards. 

 

- Mehul Patel

0 项奖励
回复

1,034 次查看
Joao_Roscoe
Contributor III

Unfortunately, no success, so far.

The installaller is still stuck right after entering the activation code - it is still asking for an activation code to be enterered in a PopUp windows.

The activation code I'm using is:

E4B4-65D0-472A-8C83

(received by e-mail from NXP)

The installation dir contains only a "jre" directory - so there are no logs.

And I'm trying to install S32DS 3 - so, I guess this does not apply.

I'm puzzled...

João

 

0 项奖励
回复

1,024 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @Joao_Roscoe , 

 

As I see on the license server there is no activation attempt. 

 

Please can you check again, reinstallation with administrator privileges right. It could be also because there was some server issue last week. Please can you give try again if it works. 

 

Thank you. Best regards. 

- Mehul Patel 

0 项奖励
回复