S32DS for Power - Cant start debug session on Win10 laptop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS for Power - Cant start debug session on Win10 laptop

1,345 Views
uditsalunke
Contributor III

S32DS for PowerPc (DevKit 5748g) - Installation on Win10 wont allow debugging over OpenSDA.

GDB debug session could not be started. The same version works fine on Win 7. 

While installing S32DS, installer through error that Jungo Connectivity Driver is not "digitally signed" and so windows 10 won't allow   debugging session to start. 

Any one facing this issue? 

0 Kudos
Reply
2 Replies

1,124 Views
uditsalunke
Contributor III

I updated P&E drivers as per P&E tech support and it fixed the issue.

Udit

0 Kudos
Reply

1,124 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried start debug session on Win10 64bit Pro version (fresh install) - and everything is working properly. Did you allow access for PE micro debug server in firewall settings? 

Jiri

0 Kudos
Reply