Hi
I am using S32 Design Studio for Power Architecture, Version: 2017.R1, Build id: 171018 together with PEmicro Multilik Universal FX. Running on Win10 Version 1803 for x64 with latest update (2018-11-19).
Target platform is the MPC5777C.
I did a project some month ago that worked well. Now I want to continue working with the test program, but it is not compiling any more. :smileyplain:
Warnings:
Invalid project path: Referenced project is not accessible. test_5777_Z7_0 pathentry Path Entry Problem
... together with...
11:02:40 **** Incremental Build of configuration Debug for project test_5777_Z7_0 **** make -j4 all 3 [main] make 9800 child_info_fork::abort: C:\NXP\S32DS_Power_v2017.R1\utils\msys32\usr\bin\msys-gcc_s-1.dll: Loaded to different address: parent(0x1C0000) != child(0x1A0000) make: fork: Resource temporarily unavailable 11:02:40 Build Finished (took 188ms)
I have cheked the Project -> Properties -> ... Build Variables like project path etc. but everything looks normal.
Does anybody has an idea what's going wrong?
Thanks and best regards
Felix
已解决! 转到解答。
Hi,
thanks for the response. The latest windows update (2018-11-29 KB4467682) solved the problem over the weekend.
Win10 is a nightmare in my view...
Best regards
Felix
#closed