S32DS Demo Project for MPC5777C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS Demo Project for MPC5777C

2,262 Views
dega
Contributor II

Hi,

are there any demo projects for the MPC5777C created in S32DS?

I would like to open the Example_MPC5777C-PinToggleStationery but it doesn't work. 

Which is the tool used to create all the demos there?

 

 

Thanks,

Marco

Labels (1)
4 Replies

1,688 Views
stanish
NXP Employee
NXP Employee

FYI: I've just created multi-core pin toggle example.

Example MPC5777C Single ELF multi-core Pin Toggling - S32DS Power v1.2 

hope it helps.

Stan

1,687 Views
dega
Contributor II

If someone is interested in the same topic I created a simple project with a PWM single channel output using the EtpuB:

Channel0 : PWMMAC,

Channel1: Bottom

Channel2: Top

0 Kudos
Reply

1,687 Views
vrushalitaklika
Contributor III

Hi Macro,

I was referring your etpu project.

I have some queries here, can you share details

1. What is the use of PIN_PT12,PT13,PT14,PT15 pins here ?

Thanks

Vrushali

0 Kudos
Reply

1,687 Views
martin_kovar
NXP Employee
NXP Employee

Hello Marco,

Unfortunately, we do not have created any example project in S32DS for MPC5777C yet.

The project you had downloaded and tried to import is created in Multi IDE from Green Hills. Please see following link.

Real-Time Operating Systems (RTOS), Embedded Development Tools, OptimizingCompilers, IDE tools, Debu... 

Bad news is, that this IDE is under license.

I hope I will have a little bit of time to convert some of the examples for S32DS soon.

Regards,

Martin

0 Kudos
Reply