S32DS 3.5_RTD3.0.0_S32K344_添加QSPI出错

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32DS 3.5_RTD3.0.0_S32K344_添加QSPI出错

259 次查看
harryoceana
Contributor II

S32DS 3.5_RTD3.0.0_S32K344_添加QSPI出错

应该怎样才能正确添加QSPI呢?

harryoceana_0-1719379301791.png

 

0 项奖励
回复
3 回复数

245 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @harryoceana,

This issue is probably caused by a faulty installation. Could you confirm the RTD package is installed correctly? Try importing the Qspi example firstly:

Julin_AragnM_0-1719424599771.png

Julin_AragnM_1-1719424633539.png

Best regards,
Julián

0 项奖励
回复

225 次查看
harryoceana
Contributor II

https://community.nxp.com/t5/S32K/S32K344-RMII-QSPI/m-p/1416828

In this post, can't RMII and QSPI be used at the same time, and can't 257BGA package be used at the same time?

Can RMII and QSPI be used at the same time if the chip pin meets the requirement of using RMII and QSPI at the same time?

harryoceana_0-1719552979254.png

harryoceana_1-1719553024367.png

 

 

0 项奖励
回复

183 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @harryoceana,

As you mentioned due to the pad type support RMII + QPSI is not possible for S32K344 devices. It is the same as it is not related to the package. You can look at the tab in the "S32K344_IOMUX.xlsx", where the ethernet use cases are listed:

Julin_AragnM_0-1719950916207.png

Best regards,
Julián

0 项奖励
回复