S32DS 1.3 for ARM integrating S32K SDK 0.8.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS 1.3 for ARM integrating S32K SDK 0.8.1

1,162件の閲覧回数
stevesun
NXP Employee
NXP Employee

Hi,

 

S32DS 1.3 for ARM comes with S32K SDK 0.8.2, is it possible to integrate S32K SDK 0.8.1 with S32DS 1.3 for ARM, so that customer can just keep one IDE S32DS 1.3 and call different SDK version to support different MCU versions.

 

Thank you!

 

Regards,

Steve

ラベル(1)
タグ(3)
0 件の賞賛
2 返答(返信)

861件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Steve,

Currently it’s not trivial to do so – and our recommendation would be to utilize the S32DS with the SDK version that was provided with it. You can have more versions of S32DS installed on the same machine.

We have this feature in consideration for S32 SDK 0.9.0 release.

Regards,

Stanislav

861件の閲覧回数
stevesun
NXP Employee
NXP Employee

Hi Stanislav,

Got it with thanks!

Regards,

Steve

0 件の賞賛