S32DS 1.3 for ARM integrating S32K SDK 0.8.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS 1.3 for ARM integrating S32K SDK 0.8.1

1,137 Views
stevesun
NXP Employee
NXP Employee

Hi,

 

S32DS 1.3 for ARM comes with S32K SDK 0.8.2, is it possible to integrate S32K SDK 0.8.1 with S32DS 1.3 for ARM, so that customer can just keep one IDE S32DS 1.3 and call different SDK version to support different MCU versions.

 

Thank you!

 

Regards,

Steve

Labels (1)
Tags (3)
0 Kudos
2 Replies

836 Views
stanish
NXP Employee
NXP Employee

Hi Steve,

Currently it’s not trivial to do so – and our recommendation would be to utilize the S32DS with the SDK version that was provided with it. You can have more versions of S32DS installed on the same machine.

We have this feature in consideration for S32 SDK 0.9.0 release.

Regards,

Stanislav

836 Views
stevesun
NXP Employee
NXP Employee

Hi Stanislav,

Got it with thanks!

Regards,

Steve

0 Kudos