S32 design studio for S32 platform 3.4 installation failed (Windows 11)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 design studio for S32 platform 3.4 installation failed (Windows 11)

Jump to solution
1,860 Views
CoderSun
Contributor I

Hello everyone,

I had the following problem while installing S32 Design Studio for Platform 3.4.

The screenshot below:

CoderSun_0-1642399454990.png

The log file below:

Install Uninstaller: S32 Design Studio for S32 Platform 3.4(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Uninstall Folder: D:\NXP\S32DS.3.4\jre
Status: SUCCESSFUL

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\FNPLicensingService
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\cll\x64
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\cll\i86
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\Xun Sun\AppData\Local\Temp\291549.tmp\cll
Status: WARNING
Additional Notes: WARNING - The path does not exist

0 Kudos
Reply
1 Solution
1,770 Views
mikedoidge
NXP Employee
NXP Employee

Hello Cylus,

The S32 Design Studio does not yet support Windows 11. No testing has been done for this. It is unknown what issues might arise from this. I suggest you look for a compatibility mode option on the installer file, perhaps that will resolve this error?

Best Regards,

Mike

View solution in original post

1 Reply
1,771 Views
mikedoidge
NXP Employee
NXP Employee

Hello Cylus,

The S32 Design Studio does not yet support Windows 11. No testing has been done for this. It is unknown what issues might arise from this. I suggest you look for a compatibility mode option on the installer file, perhaps that will resolve this error?

Best Regards,

Mike