S32 Design Studio for Power Architecture v1.1 installation problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Power Architecture v1.1 installation problem

1,545 Views
yankuang1
Contributor III

I'm trying to install S32_Power_Linux_v1.1.bin on linux(Ubuntu12.04),but it does not ask me to inser the activation ID  and unroll the installation.

177864_177864.pngpastedImage_2.png177856_177856.pngpastedImage_3.png

177865_177865.pngpastedImage_4.png

0 Kudos
Reply
4 Replies

1,277 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS team replied that only 64 bit Linux systems are supported. I recommended highlighting this info in feature list and release notes. Based on this PDF - s32ds.pwr.linux.quick_start.pdf  - some 32 bit libraries must be installed  (lib32z1, lib32ncurses5 and lib32bz2-1.0).

Jiri 

0 Kudos
Reply

1,277 Views
yankuang1
Contributor III

Hi,

Thank you very much.I tried download this document,but  i Can't open this link.

0 Kudos
Reply

1,277 Views
jiri_kral
NXP Employee
NXP Employee

Sorry - it looks like that link above is for internal purposes only. The file is in attachment. 

0 Kudos
Reply

1,277 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried install it on Ubuntu 12.04 and 14.04 - and ended with the very same messages in the log - even with root privileges. I'm able install it on Debian 8 and Ubuntu 16.04. I'm going to create ticket for S32DS team.   

0 Kudos
Reply