S32 Design Studio for Arm stuck at Licenses Verification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for Arm stuck at Licenses Verification

1,975件の閲覧回数
jtro
Contributor III

S32 Design Studio for Arm stuck at Licenses Verification. Did everything but it does not move ahead.

Also tried to cancel the operation but it doesn't work.

Even after Re installation doesn't help it shows the same message.

Not able to access any menu or option. Please help

 

S32 error.jpg

0 件の賞賛
返信
3 返答(返信)

1,966件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

this is known issue and dev team is working on that. Hope they will have solution soon. If it is urgent - please create NXP support ticket. There is workaround, but it requires your email address used in NXP account. Or you can send it to me in a private message (will be probably faster). 

 

Jiri

0 件の賞賛
返信

1,923件の閲覧回数
chen_gilbert
Contributor II

Hi @jiri_kral 

Does this issue impact to all s32ds? I can duplicate this issue on s32ds 3.2, s32ds 3.3 and s32ds for ARM Version 2018.R1.

If possible, can you share the workaround to my account chen.gilbert@inventec.com

thanks,

Gilbert

1,917件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Gilbert, 

 

here is the workaround procedure: 

Please use the next workaround to disable "Extension and Updates" to check update site.
1) go to ARM product instllation directory;
2) then "eclipse\configuration\.settings" folder
3) open in editor file "com.nxp.s32ds.rcp.modular.core.prefs" 
4) modify line from "showOnStartUp=true" to "showOnStartUp=false"
5) launch ARM product.

After this you can use your S32DS. If there is still message about expiration date (all Expiration dates was moved to 2025) - you need to refresh your License (Help->NXP Licenses) 

jiri_kral_0-1612443202477.png

 

Jiri

 

 

0 件の賞賛
返信