S32 Design Studio for Arm stuck at Licenses Verification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Arm stuck at Licenses Verification

1,973 Views
jtro
Contributor III

S32 Design Studio for Arm stuck at Licenses Verification. Did everything but it does not move ahead.

Also tried to cancel the operation but it doesn't work.

Even after Re installation doesn't help it shows the same message.

Not able to access any menu or option. Please help

 

S32 error.jpg

0 Kudos
Reply
3 Replies

1,964 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this is known issue and dev team is working on that. Hope they will have solution soon. If it is urgent - please create NXP support ticket. There is workaround, but it requires your email address used in NXP account. Or you can send it to me in a private message (will be probably faster). 

 

Jiri

0 Kudos
Reply

1,921 Views
chen_gilbert
Contributor II

Hi @jiri_kral 

Does this issue impact to all s32ds? I can duplicate this issue on s32ds 3.2, s32ds 3.3 and s32ds for ARM Version 2018.R1.

If possible, can you share the workaround to my account chen.gilbert@inventec.com

thanks,

Gilbert

1,915 Views
jiri_kral
NXP Employee
NXP Employee

Hi Gilbert, 

 

here is the workaround procedure: 

Please use the next workaround to disable "Extension and Updates" to check update site.
1) go to ARM product instllation directory;
2) then "eclipse\configuration\.settings" folder
3) open in editor file "com.nxp.s32ds.rcp.modular.core.prefs" 
4) modify line from "showOnStartUp=true" to "showOnStartUp=false"
5) launch ARM product.

After this you can use your S32DS. If there is still message about expiration date (all Expiration dates was moved to 2025) - you need to refresh your License (Help->NXP Licenses) 

jiri_kral_0-1612443202477.png

 

Jiri

 

 

0 Kudos
Reply