S32 Design Studio for ARM license expiring in 13 days

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for ARM license expiring in 13 days

ソリューションへジャンプ
15,277件の閲覧回数
609510318
Contributor I

S32 Design Studio for ARM license expiring in 13 days,how can i solve it?Thanks!

 

S32 Design Studio for ARM

ActivationId: F625-BD17-9FB6-009D
Evaluation Days: 13
Feature Version: 2.2
Feature Status: Evaluation (13 days)

0 件の賞賛
1 解決策
15,156件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

I have returned your license, when you re-activate, the new expiration date will be loaded.

Best Regards,

Mike

元の投稿で解決策を見る

0 件の賞賛
67 返答(返信)
6,043件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @Bryan9,

I've extended yours. Please try the Refresh option in the license menu of S32 Design Studio.

Best regards,

Mike

0 件の賞賛
6,012件の閲覧回数
Bryan9
Contributor I

@mikedoidge,

I tried it, but the license menu shows me the following error:

Lic.png

0 件の賞賛
5,723件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @Bryan9,

Sorry about that. It's extended now. Please try again.

Mike

0 件の賞賛
5,702件の閲覧回数
Bryan9
Contributor I

@mikedoidge,

I tried again, but the same error occurs.

0 件の賞賛
5,562件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Bryan9,

I checked the license server, there was one user able to re-activate with updated expiration date. It only gives me an encrypted machine ID so I cannot tell who. There were a number (about 20) of expired licenses from prior activations. I manually returned them so now there is just the 1 license. Try again. If that doesn't work, your trusted storage may be corrupted and needs to be re-initialized. To correct this:

Windows host:

-> Delete 'C:\ProgramData\FLEXNet'

 

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

Linux host:

/usr/local/share/macrovision/storage

 

Best regards,

Mike

0 件の賞賛
5,525件の閲覧回数
Bryan9
Contributor I

Hi @mikedoidge,

Works now.

Thank you so much for your help!

0 件の賞賛
6,034件の閲覧回数
thomaswhitburn
Contributor I

I have the same problem.   Can I have my license for S32 Design Studio for ARM V2.0 extended?

0 件の賞賛
5,121件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Thomas, 

Your license expire on 9/22/2026. Please return existing license and activate S32DS again. 

 

Jiri

0 件の賞賛
5,867件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @thomaswhitburn,

I checked your account. You have an entitlement which is valid through 2026. There are no licenses listed. So either you haven't activated it yet, or you successfully returned the license(s) you did have. Is there an issue I could help you with?

Best Regards,

Mike

0 件の賞賛
5,860件の閲覧回数
thomaswhitburn
Contributor I

I see an entitlement and license expiration of 9/22/21 in my License List page.  When I try to use the old activation code in the IDE I get this error:

thomaswhitburn_0-1632409361980.png

 

0 件の賞賛
5,759件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @thomaswhitburn,

I understand now. You are still using the v2.0, even though you now also have the v2.2.

I will extend your entitlement for the v2.0, but I encourage you to upgrade to the v2.2. However, if you are working with the S32K1xx family devices, I would recommend that you migrate to the S32 Design Studio for S32 Platform v3.4. This is our latest version and is upon which the recent and future updates have been and will be made going forward.

Best Regards,

Mike

0 件の賞賛
5,989件の閲覧回数
cheoljin
Contributor II

My license also expired. 

Would you extend it ? 

Best Regards, 

Cheol Jin.

0 件の賞賛
6,416件の閲覧回数
p_a_u_darshana
Contributor III

Hi,

My license is expired already. How can I get the new license key from the download page?

Or is there any way to update the current license?

Thank you.

0 件の賞賛
6,322件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

@p_a_u_darshana,

Your license has already been extended through 2025.

I checked your account and manually returned the expired license. Now you just need to re-activate using the same activation code you used before. It was provided to you via email and as well you can locate it from the download site after you log on NXP.com

Please let us know of any further difficulties.

Best Regards,

Mike

6,618件の閲覧回数
609510318
Contributor I

Thanks.I try to  return  license, but the error happens as follows.Could you help me to solve it?

QQ截图20210214102040.png

0 件の賞賛
15,157件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

I have returned your license, when you re-activate, the new expiration date will be loaded.

Best Regards,

Mike

0 件の賞賛
1,290件の閲覧回数
Romeo
Contributor I

Hi Mike,

I made an automotive product using S9KEAZN8AMFK.
I know that S9KEAZN8AMFK is AEC-Q100 Grade 1.
And the company we supply products to says they need an AEC-Q100 Grade 1 certification test report.
I must submit proof that S9KEAZN8AMFK is AEC-Q100 Grade 1.

Can you send me the AEC-Q100 Grade 1 certification test report?

Best Regards,

romeo

0 件の賞賛
1,776件の閲覧回数
JunSeoHan
Contributor I

Can I get my license renewed for S32 Design Studio for Power Architecture version 2.1

License Quantity: 1
Fulfillment ID: 204206657
Expiration Date: Jul 25, 2023
Product: S32DS-PA_v2.1
Machine: 483388A23C18B58170F1C714DC44DCB778407246
Activation Code: 1F53-8519-116C-C730

 

0 件の賞賛
1,746件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @JunSeoHan 
I have extended your license through end of December - 2026.

Please re-activate it, so the new expiration date will be loaded.

Best Regards,

- Mehul

0 件の賞賛
3,311件の閲覧回数
chrislin_wpi
Contributor II

Dear Mike,

My license is also expired.

Would you please help me?

 

S32 Design Studio for S32 Platform

ActivationId: 6BE2-D0D8-F807-B0E7
Evaluation Days: 1431
Feature Version: 3.4
Feature Status: Evaluation (1431 days)

0 件の賞賛
3,303件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi Chris,

This license is not expired. As you point out it is valid for 1431 days. What is the issue you are having?

Mike

0 件の賞賛