S32 Design Studio for ARM license expiring in 13 days,how can i solve it?Thanks!
S32 Design Studio for ARM
ActivationId: F625-BD17-9FB6-009D
Evaluation Days: 13
Feature Version: 2.2
Feature Status: Evaluation (13 days)
解決済! 解決策の投稿を見る。
I have returned your license, when you re-activate, the new expiration date will be loaded.
Best Regards,
Mike
Hi @Bryan9,
I've extended yours. Please try the Refresh option in the license menu of S32 Design Studio.
Best regards,
Mike
I tried again, but the same error occurs.
Hello @Bryan9,
I checked the license server, there was one user able to re-activate with updated expiration date. It only gives me an encrypted machine ID so I cannot tell who. There were a number (about 20) of expired licenses from prior activations. I manually returned them so now there is just the 1 license. Try again. If that doesn't work, your trusted storage may be corrupted and needs to be re-initialized. To correct this:
Windows host:
-> Delete 'C:\ProgramData\FLEXNet'
This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.
Linux host:
/usr/local/share/macrovision/storage
Best regards,
Mike
I have the same problem. Can I have my license for S32 Design Studio for ARM V2.0 extended?
Hi Thomas,
Your license expire on 9/22/2026. Please return existing license and activate S32DS again.
Jiri
Hi @thomaswhitburn,
I checked your account. You have an entitlement which is valid through 2026. There are no licenses listed. So either you haven't activated it yet, or you successfully returned the license(s) you did have. Is there an issue I could help you with?
Best Regards,
Mike
I see an entitlement and license expiration of 9/22/21 in my License List page. When I try to use the old activation code in the IDE I get this error:
Hi @thomaswhitburn,
I understand now. You are still using the v2.0, even though you now also have the v2.2.
I will extend your entitlement for the v2.0, but I encourage you to upgrade to the v2.2. However, if you are working with the S32K1xx family devices, I would recommend that you migrate to the S32 Design Studio for S32 Platform v3.4. This is our latest version and is upon which the recent and future updates have been and will be made going forward.
Best Regards,
Mike
My license also expired.
Would you extend it ?
Best Regards,
Cheol Jin.
Hi,
My license is expired already. How can I get the new license key from the download page?
Or is there any way to update the current license?
Thank you.
Your license has already been extended through 2025.
I checked your account and manually returned the expired license. Now you just need to re-activate using the same activation code you used before. It was provided to you via email and as well you can locate it from the download site after you log on NXP.com
Please let us know of any further difficulties.
Best Regards,
Mike
Thanks.I try to return license, but the error happens as follows.Could you help me to solve it?
I have returned your license, when you re-activate, the new expiration date will be loaded.
Best Regards,
Mike
Hi Mike,
I made an automotive product using S9KEAZN8AMFK.
I know that S9KEAZN8AMFK is AEC-Q100 Grade 1.
And the company we supply products to says they need an AEC-Q100 Grade 1 certification test report.
I must submit proof that S9KEAZN8AMFK is AEC-Q100 Grade 1.
Can you send me the AEC-Q100 Grade 1 certification test report?
Best Regards,
romeo
Can I get my license renewed for S32 Design Studio for Power Architecture version 2.1
License Quantity: 1
Fulfillment ID: 204206657
Expiration Date: Jul 25, 2023
Product: S32DS-PA_v2.1
Machine: 483388A23C18B58170F1C714DC44DCB778407246
Activation Code: 1F53-8519-116C-C730
Hi, @JunSeoHan
I have extended your license through end of December - 2026.
Please re-activate it, so the new expiration date will be loaded.
Best Regards,
- Mehul
Dear Mike,
My license is also expired.
Would you please help me?
S32 Design Studio for S32 Platform
ActivationId: 6BE2-D0D8-F807-B0E7
Evaluation Days: 1431
Feature Version: 3.4
Feature Status: Evaluation (1431 days)
Hi Chris,
This license is not expired. As you point out it is valid for 1431 days. What is the issue you are having?
Mike