I have returned your license, when you re-activate, the new expiration date will be loaded.
Best Regards,
Mike
Dear Mike,
I installed the S32 Design Studio for S32 Platform, it shows my license expiring.
Because I didn't get a valid license to install Extensions and Updates.
I had refresh, but it still fail.
I also check my license on the NXP.com website, but it shows Expiration Data is 2026/4/6
Hi,
I'm not sure what's the issue - if you stretch a little bit the column with Message License Expiring... you will probably see something like this:
Means your license will expire after 4 years.
What particular issue do you have - can you please share a screenshot with error message? Which update/package you can't install?
Jiri
Hi Mike:
can you also help to return my license,thanks!
License Applicable to Product(s): Version Description 2.2 S32 Design Studio for ARM v2.2
License Quantity: 1
Fulfillment ID: 175776437
Expiration Date: Jul 29, 2021
Product: S32 Design Studio for ARM v2.2
Machine: CF30D5D79DD2230677821310B765396A863F0550 Activation
Code: 919B-D4D4-4E64-0434
Hi Bevan,
Your entitlement expiration is in 2025, probably you just need to refresh the license in S32 Design Studio. Also, you could return the license and re-activate. Sometimes it's not possible to do either. If this is the case for you, I can return the license on the server side. Just let me know.
Best Regards,
Mike
Hi mike.
Can you also refresh my license for S32 Design Studio for ARM 2.2 ?
License Quantity: 1
Expiration Date: Jul 6, 2021
Code: 01D6-1D4C-0851-E4A9
I can't return the license, and it is not possible to re-install this software again.
Or, let me know how to re-activate the license.
Best regards.
Can I get my license renewed for S32 Design Studio for ARM 2.2
The license has expired.
Thanks,
Stephan
Hello @stephandewit1,
I have returned your expired license, but the entitlement was already extended. Just re-activate with same activation code and you will receive a new license.
Best regards,
Mike
I have the same problem. Can you please re-activate my licence?
Fulfillment ID: 152126887
Expiration Date: Nov 7, 2021
Product: S32 Design Studio for PA E200
Machine: CB93635434074A5B26076ED3A12D8E2F204A0001
Activation Code: 9441-28CA-C473-A597
Hello @jackeyhong ,
I have returned your license on the server, please re-activate the same activation code you already have. It will then show the new expiration date.
Best Regards,
Mike
Hello @Sunnny,
You can continue to use your current activation code. The existing license was extended on the server, but the tools on you PC did not get updated expiration date so it is necessary to return and then re-activate to receive the new date.
Best Regards,
Mike